SmartSound™ MEMS Microphones

phpbb forum ID
34116
By kumarsoftiocom , 14 February 2024

Hello. Is T5848 real and available for purchase? We have a need for an I2S mems microphone with AAD support for a battery powered device. Currently using a different offshore I2S mems microphone for the proof of concept. Raised a request over a week ago and so far no reply. We have a limited timeline for this evaluation and will appreciate direct contact details and/or information on the availability of this new product that was announced a while ago. Thanks.

By peterchen3hone… , 15 January 2024

I have learned that you have an All-in-one microphone evaluation module development board, model MD-54001-D58 supports analog microphone connection. Support model EV_ICS-40720-FX flexible development board, I in the technical documentation in any case cannot find how to connect them together, because the analog microphone EV_ICS-40720-FX pins and numbers are different, the documentation does not give how to connect the analog microphone. How can I connect them together?

By tejashripradha… , 4 January 2024

Are you attending CES 2024? Make sure you visit us at booth #20521! Come to our booth and be part of our groundbreaking hearables demonstration. Join the TDK team in stepping into the sound of the future.

By mohandmoussace… , 7 December 2023

I’m working with the SmartSound one development board, with the T5837 eval. When I record with Audacity or in python the microphone does not record the entire track that I play. For example I play a frequency sweep from 20Hz to 8000Hz in 10 seconds. The microphone does not record the entire sweep, it cuts at a certain frequency which changes each time. it's as if there was a noise reduction function that activates and deactivates.

By kabeeraiahalarmcom , 29 November 2023

Can I get a sample application code to test the MIC wakeup feature supported in the T5838 microphone, I am looking to configure the registers through a 1-wire protocol and to test the wake-up feature.