Hello
I am seeing substantial (between 10 and 20 m/s**2) low frequency (i.e. remains after an aggressive 10Hz cutoff filter) non-zero mean noise on an MPU9250 accelerometer. In the time domain, the noise shows up as "impulses" -- the signal will be mostly concentrated around 0 (as expected), and then occasionally will spike up to high values, before returning to roughly 0. The spikes are always in the same direction. The signals are observed on many (>10) different boards, and are observed independent of the IMU config parameters (DLPF settings & scale).