SmartMotion eMD Output Units

By tkeady5gmailcom , 5 April 2023

It doesn't seem to be clearly defined in the software examples what units the outputs are in. Is acceleration milli-Gs or Gs, angular rate degrees or radians per second, or something else, etc.

I'm specifically referring to the file source/examples/example-high-rate-logger.py from the following links: https://invensense.tdk.com/developers/download/dk-42688-p-smartmotion-emd-2-0-3/?wpdmdl=38397
https://invensense.tdk.com/developers/download/dk-42605-smartmotion-emd-2-0-1/?wpdmdl=37477

Is it dependent on the firmware programmed onto the development board? Which is also included in the above files. If so, where in the Atmel studio code? Thank you.

Nickname
jaymins

jayminshah1tdkcom

2 years 10 months ago

Yes it is dependent on firmware programmed. Please look at atmel solution file in ..sources\examples\example-high-rate-logger.
The units are g and dps.

phpbb Post ID
44946
phpbb Topic ID
39248