SmartIndustrial™ Industrial MEMS Motion Sensors

phpbb forum ID
39764
By alfredoagenjoa… , 10 September 2024

The following is said about IIM-46234: "The performance of the thermal related specification was improved by performing custom thermal calibration for every module in the temperature range (-40 to 85°C)."
I understand this means that the thermal bias is achieved to be 0 when the sensor is at 25 ºC.
Are the measured biased (in the temperature range -40 to +85ºC) provided to the user along with the unit, for each bought unit?
(that info, if provided, can be used by the user to compensate the bias with the measured temperature for the IIM-46234)

By fabian181096gmailcom , 9 July 2024

Hello TDK support

Our company is using the iim42652 sensor with a custom driver to implement a "shock detection".
When the MCU goes to a low power hibernation mode, it should be woken up again when there is a sudden high acceleration.
The WOM and SMD feature of the iim42652 seems to fit our purpose.

By guptaembeddedg… , 2 April 2024

Hi,

I am trying to interface IIM-42352 with our TI controller, I am able to use SPI interface between them and run example-self-test and example-raw-data-registers successfully. But when I am testing the example-raw-data, the accel and temp data read from FIFO is constant even when I am moving the sensor. I suspect the issue might be the way the example reads the FIFO is incorrect or FIFO not getting updated with latest values.

By tempxquancomtw , 24 February 2024

We have produced thousands of vibration sensors with IIM-42351 and IIM-42352. We don't find any problem in the development stage. However, after deployment, our customer reports malfunctions and defects. The issues with defects are mainly divided into two categories.
First, some sensors' out value for the Z axis is stuck at 32767 (the maximum possible output value for a 16-bit integer). With some impact on the sensor, measurement can be back to normal. But is easily stuck again at times.
Second, the measurement value may drift more than 10% in a month for some sensors.

By emanuelkaspere… , 16 February 2024

We would like to use the IIM-42351 with an external clock.
The IIM-42351 is powered with 3.3V. Unfortunately, the data sheet does not clearly indicate which minimum and maximum voltage is possible at the CLKIN input.
Can someone help me?
For example, I would like to use a SIT1533.
Thanks in advance

By tejashripradha… , 4 January 2024

Are you attending CES 2024? Experience design versatility and superior functioning with our two latest IMUs. Our SmartMotion IMU is ideal for IoT applications while our SmartIndustrial IMU enhances accuracy for drones and navigation systems.

Make a stop at our booth #20521 for a comprehensive understanding. See you there!

By evanwtfhivemappercom , 15 November 2023

Hello,

We have ~10,000 devices with a iim 42652 and are looking to provide a software update to our users to better utilize the IMU capabilities. Unfortunately, we are not currently calibrating the IMUs.

Our devices are communicating with the IMU directly via SPI.

We have been reading through the data sheet and the eMD documentation, but would really appreciate some guidance on a path forward for utilizing the example code to properly calibrate the gyroscope, etc. (like in 5.2 Example Algorithm or 5.9 SELF-TEST EXAMPLE)