SmartAutomotive™ Automotive MEMS Motion Sensors

phpbb forum ID
39767
By marcocastell74 , 4 October 2024

Review of the technical datasheet does not reveal significant differences between the IAM-20680HT and IAM-20680HP devices.
Will you please explain at the high-level if there is a difference in the testing and selection that parts undergo to be categorized HT vs HP?
And are there some functions that are not enabled in one device vs the other?

By akotelnikovcog… , 3 October 2024

Hello, community, I hope, that somebody has a solution for this.
I've faced a situation in which sometimes randomly z axis of the IAM-20680 gyro axis becomes stuck.
As on the picture below (sticked axe in rest.jpg) you can see that in rest all of the axis show pretty the same behaviour in terms of range of noise.
But when I'm starting to rotate the IMU around all of 3 axis, one of them shows the same values as it would be in rest (you can see it on the sticked axe in moving.jpg - line wz).

By gaurisawantgen… , 24 May 2024

IAM20680 giving 0 on X and Z axis and 3 on Y axis when it is at rest.
Gyro sensitivity is 131 LSB/dps (FS_SEL = 0) and accelerometer is 16,384 LSB/g (AFS_SEL=0).
I'm recording 200 samples at every 10ms and then calculating average of it, to calculate gyro and accel values.
I don't know how to verify gyro values as well.
I've attached a screenshot of results, I have also attached ST and normal mode results at rest. Please help me out.

By tejashripradha… , 4 January 2024

Are you attending CES 2024? Join us as we unveil our newest addition to the InvenSense SmartAutomotive™ product line, the groundbreaking 3-axis MotionTracking™ accelerometer, now fully operable up to 105°C.

Don't miss the chance to experience a live demonstration at our booth #20521!

By qshanparacommcouk , 2 August 2023

Hi Everyone,
I am using EV-IAM-20380HT board to evaluate IAM-20380 Gyroscope. I have following issues with EV-IAM-20380HT:
1. can not find the datasheet of EV-IAM-20380HT, however, the datasheet of IAM-203380 is available.
2. get WHO-AM-I register value is 253 (0xFD), not the 181(0xB5) as indicate in the datasheet, through I2C reading.
3. the SDA and SCK of EV-IAM-20380HT is directly connected to the master’s SDA & SCK (3.3V logic) in my application. Do the SDA and SCK need to pull up to +3.3V with 2x 10k resistors respectively?

By julianwestemvexiscom , 6 July 2023

Good evening,

We have been developing an application using the IAM-20680HT and HP devices for ~18 months, but have started to notice recently issues matching the acceleration values from the IAM devices, to other accelerometers used in our product.

We think the issue may be related to filter attenuation. The datasheet does not specific if the low pass filter is a 2, or 4 pole filter - and thus wether the roll off rate is 20dB/decade, or 40dB/decade - please may you confirm?

By petrihaavistos… , 27 January 2023

Hi,

We are using the IAM-20380 gyroscope in a small low power device and I am trying to optimize power consumption. In some cases the sleep mode is too slow to react and I need to use the next best thing, but I am not sure what it is.
My assumption is the standby-mode (Power mgmt 1 register 107, bit 4). But there seems to be no information about the power consumption of that mode in the data sheet. Table 2 of the data sheet lists power consumptions, but not for standby.