InvenSense® Introduces Comprehensive Portfolio of Disruptive New Digital and Analog Microphones

By admin , 6 January 2015
Description

SAN JOSE, Calif.--(BUSINESS WIRE)--Jan. 6, 2015-- InvenSense, Inc. (NYSE:INVN), the leading provider of intelligent sensor solutions, announced at the 2015 Consumer Electronics Show the release of six (6) new state-of-the-art microphones to address the needs of the Mobile, Wearable, IoT, Smart TV and Bluetooth headset markets. InvenSense’s new microphone portfolio enables OEM partners to differentiate their product offerings by improving the consumer experience with increased speech clarity and high fidelity recordings while reducing size and remaining cost competitive with today’s existing solutions.

InvenSense introduces the world’s smallest size analog MEMS microphone at 65 dB SNR performance:

ICS-20100 is the world’s smallest MEMS microphone delivering 65 dB SNR in a bottom port package and targets mobile electronic devices such as noise cancelling Bluetooth headsets, smartphones, and in-ear wearable devices. The ICS-20100 achieves its impressively small 4.5mm2 footprint by utilizing the patented and production proven InvenSense Fabrication Process. The ICS-20100 will be sampling in 1H of CY2015.

InvenSense announces the world’s lowest power PDM microphone:

The ultra-low power ICS-41350 enables the transition of microphones from analog to digital as required by ‘AlwaysOn’ applications in smartphones, tablets, remote controls, smart TVs, Bluetooth headsets and digital still/video cameras. The ICS-41350 is a multi-mode, low noise, bottom ported MEMS microphone in a 3.5 mm x 2.65 mm x 0.98 mm package. The ICS-41350 offers an exceptionally efficient 175 µA ultra-low power mode, high SNR of 66 dB, high Acoustic Overload Point (AOP) of 126 dB and ultrasonic band support for gestures and other creative uses. The ICS-41350 will sample in 1H of CY2015.

InvenSense is also introducing two sets of high performance analog microphones with matching electro-acoustic performance for both top and bottom port devices.

ICS-40618 and ICS-40619 are matching analog microphones and achieve industry leading SNR performance of 68 dB as well as a high AOP of 132 dB SPL for mobile applications where there is a demand for highest performance in a constrained size. In the ultra-low power mode when the supply voltage is below 2 V, the microphones consume less than 70 µA allowing the longest ‘AlwaysOn’ standby times and best-in-class performance. The ICS-40618 (bottom port) and ICS-40619 (top port) are available for sampling in a small 3.5 mm x 2.65 mm x 0.98 mm surface mount package. The ICS-40618 and ICS-40619 matching solution will be sampling in Q1 of CY2015.

ICS-40180 and ICS-40181 are matching analog microphones providing industry leading RF immunity performance, SNR of 65 dB, extended AOP of 124 dB SPL and excellent acoustic matching response. The solutions enable beamforming which allows end-users to suppress surrounding noise and audio “zoom” into desired conversations. The ICS-40180 (bottom port) and ICS-40181 (top port) dual microphone solutions are available now in a 3.5 mm x 2.65 mm x 0.98 mm surface mount package and are targeted for smartphones and slim consumer electronic devices. The ICS-40180 and ICS-40181 matching solution are available now for sampling.

“InvenSense is committed to bringing to market a broad portfolio of disruptive, high performance and innovative Audio solutions,” said Ali Foughi, VP of Marketing and Business Development. “By applying numerous MEMS technological breakthroughs, we have developed the industry’s only I²S microphone, the lowest power PDM, ultra-low power analog, the world’s smallest footprint microphone at 65dB performance, and the industry’s leading SNR performance thus enabling our customers to create a differentiated audio experience.”

InvenSense is exhibiting in booth #35806 in South Hall 4 at the 2015 Consumer Electronics Show taking place in Las Vegas, Nevada from January 6 - 9, 2015. To schedule press and partner meetings at the show, contact pr@invensense.com. For additional information and data sheets, please visit www.invensense.com or contact InvenSense Sales at sales@invensense.com.

About InvenSense

InvenSense Inc. (NYSE:INVN) is the world’s leading provider of intelligent sensor solutions for consumer electronic devices. The company’s patented InvenSense Fabrication Platform and patent-pending MotionFusion™ technology address the emerging needs of many mass-market consumer applications via improved performance, accuracy, and intuitive motion-, gesture- and sound-based interfaces. InvenSense technology can be found in consumer electronic products including smartphones, tablets, wearables, gaming devices, optical image stabilization, and remote controls for Smart TVs. The company’s MotionTracking products are also being integrated into a number of industrial applications. InvenSense is headquartered in San Jose, California and has offices in Canada, China, France, Korea, Japan, Slovakia, Taiwan, and Boston, MA. More information can be found at www.invensense.com or follow us on Twitter at @InvenSense.

©2015 InvenSense, Inc. All rights reserved. InvenSense, MotionTracking, MotionProcessing, MotionProcessor, MotionFusion, MotionApps, DMP, AAR, and the InvenSense logo are trademarks of InvenSense, Inc. Other company and product names may be trademarks of the respective companies with which they are associated.

Source: InvenSense, Inc.

 

Read Time (minutes)
4
Published Date
Image
Image