almost one second interval between each acceleration output

By tchsu , 27 September 2012

Hello,

when i cycle the sensor trough the modes with mfs and then ask for example the acceleration output with mfa i got an output rate around 1Hz, much slower than the rate if i ask for quaternions.
How do i increase that rate in the eMPL? I need accelerations in output with a 100 Hz rate at least!

Nickname
guym

guy_mcilroy

13 years 5 months ago

The data rate of the acceleration data is highly configurable, but will require a programming interface to configure. All source required to build the application is available under the download tab.

phpbb Post ID
21309
phpbb Topic ID
14715