Answer
To create and use a mapping gyro bias to temperature, using the ML_BIAS_FROM_NO_MOTION tracker to discover gyro bias and the IMU/MPU’s built in temperature sensor to determine temperature. The mapping of gyro bias to temperature will stay constant [1] throughout the lifetime of the part, so a bias, once learned, can be used to calibrate the gyro at any time it is at that temperature. When ML_LEARN_BIAS_FROM_TEMPERATURE is active, the Embedded
MotionApps Platform will store bias and temperature information discovered from ML_BIAS_NO_MOTION calibration events. When ML_BIAS_FROM_TEMPERATURE is active, stored bias and temperature information is used to update the gyro bias as temperature changes.
[1] The mapping of gyro bias to temperature is affected by mechanical stress on the sensor package. This includes stress due to soldering, tension or compression of the printed circuit board. More information is available in the IMU/MPU product specification.